콘텐츠로 건너뛰기
STAGING SERVER
DEVELOPMENT SERVER

카메라 파라미터 구성#

The pylon Viewer application allows you to configure most of the camera parameters using a graphical user interface.

The following animation demonstrates how to configure camera parameters with the pylon Viewer.

As an example, the Gain Auto auto function is set to Off 그리고 다음을 설정하십시오: Gain 및 Black Level parameter values are increased.

To quickly access the parameters, the Search feature is used.

Setting Camera Parameters (Animation)